Loading...

Powering the Future: Your All-in-One Guide to EV Series Pro Charging & Beyond

EV Series Pro Grouping

The EV Series Pro is leading the way in commercial and fleet electric vehicle charging with innovative technology, seamless integration, and user-friendly features tailored for professional environments. Designed for applications such as multifamily dwellings, workplaces, and fleet operations, this powerful solution supports any electric vehicle. This blog is your one-stop resource for everything you need to know, from understanding product specifications to mastering AmpUp software, setting up and configuring your device, and troubleshooting after installation. Get ready to power up smarter, charge faster, and simplify your EV experience like never before.

 

Technical Information on The Stations

We are first going to get into the product information for anyone unfamiliar with the EV Series Pro. On the EV48S and EV80S LCD screens, it contains charger status, output, connectivity, and additional basic charging information. For your specific EV Series Pro charger, the size circuit required for an EV48G/S is a dedicated 60 AMP breaker, an EV48S-DP is two dedicated 60 AMP breakers, while for an EV80G/S charger it requires a dedicated 100 AMP breaker. For a deeper look into those products, you can view them below:

 

Utilizing AmpUp Charging Management Software

Drivers can access your EV Pro Chargers via the QR label on the front of the unit. Within the general settings, you will be able to customize and manage important aspects of your charging stations. You can also set up your revenue payout if you’re on a Core or Pro plan. For more information regarding general settings, you can visit General Settings – Support Center. To view the analytics, you will need to go to the analytics page, where you can find a monthly breakdown of your revenue, carbon emissions, savings, utilization data, and more. Further information can be found at Analytics Page – Support Center. In the dashboard you can manage all your chargers and locations, more specifically monitoring the status of your chargers, the current load across all your locations, and which drivers are currently charging. Watch and learn how to use the EV charging management dashboard here.

 

AmpUp Benefits

The Pro plan enables sophisticated pricing and fee structures to get the most out of your EV charging investment and generate maximum returns.

Analytics & Reporting 

  •  Analytics & Reporting - View charging session data, utilization, revenue, and sustainability metrics. Download reports and analytics for utility or ESG reporting and rebates. 

Driver Access

  • Driver Reservations - Drivers can be sure a charger is available by reserving in advance.
  • Driver RFID Card
    • Charge with the tap of an RFID card. AmpUp supports adding charge to a RFID the driver already has (for example, a building badge). 
  • Location Access Control
    • Publish charging stations to the AmpUp mobile app, Google Maps, and PlugShare, or keep them private.
  • Driver Access Groups
    • Control charger access and pricing for specific groups of drivers, including free or subsidized charging.
  • Time-Based Access Control
    • Change public access based on the day and time for each location.
  • Session Limits & Idle Fees
    • Encourage drivers to share charging stations by imposing time limits or charging idle fees for drivers staying after a certain period. 

Revenue Generation

  • Revenue Collection & Direct Deposit
    • Set rates by time or energy used. Revenue collected from drivers’ charging sessions is remitted via direct deposit to a single bank account. 
  • Tiered Pricing
    • Set two-tier charging rates with one price for an initial period or energy usage and a different rate thereafter. 
  • Time-of-Use Rates
    • Manage pricing based on the time of day to accommodate for different utility rates or driver demand. 

Location & Account Management

  • Multi-Site Management
    • Manage multiple locations from one dashboard – floors of a parking garage, areas of a campus, different addresses – as unique areas with different settings.
  • Multi-User Account
    • Enable multiple users to see analytics, download reports, and manage charging by adding them as a manager or operator to the account.
  • Advanced Load Management
    • Set an energy load cap that limits the maximum power available across a location to reduce the load on the panel.

Support & Troubleshooting

  • Support
    • Drivers have 24/7 access to AmpUp’s help desk. The Pro plan includes host support via email, chat, and talk between the hours of 8am - 8pm Eastern Time. 
  • Remote Troubleshooting
    • Get alerts, diagnose problems, and remotely restart chargers.
  • Automatic SW Updates
    • AmpUp software is updated constantly with new features and improvements. By choosing AmpUp, hosts and drivers benefit from frequent updates of our products to enhance station management and charging experience.

(What is included in the PRO plan? – Support Center)

The Core plan includes the ability to take payments from drivers, enabling you to make EV charging into a business. 

Analytics & Reporting

  • Analytics & Reporting - View charging session data, utilization, revenue, and sustainability metrics. Download reports and analytics for utility or ESG reporting and rebates. 

Driver Access

  • Driver Reservations - Drivers can be sure a charger is available by reserving in advance.
  • Driver RFID Card - Charge with the tap of a RFID card. AmpUp supports adding charge to a RFID the driver already has (for example, a building badge). 
  • Location Access Control - Publish charging stations to the AmpUp mobile app, Google Maps, and PlugShare, or keep them private.
  • Driver Access Groups - Control charger access and pricing for specific groups of drivers, including free or subsidized charging.

Revenue Generation

  • Revenue Collection & Direct Deposit - Set rates by time or energy used. Revenue collected from drivers’ charging sessions is remitted via direct deposit to a single bank account. 

Location & Account Management

  • Multi-Site Management - Manage multiple locations from one dashboard – floors of a parking garage, areas of a campus, different addresses – as unique areas with different settings.
  • Multi-User Account - Enable multiple users to see analytics, download reports, and manage charging by adding them as a manager or operator to the account.

Support & Troubleshooting

  • Support - Drivers have 24/7 access to AmpUp’s help desk. The Core plan includes host support via email, chat, and talk between the hours of 8am - 8pm Eastern Time. 
  • Remote Troubleshooting - Get alerts, diagnose problems, and remotely restart chargers. 
  • Automatic SW Updates - AmpUp software is updated constantly with new features and improvements. By choosing AmpUp, hosts and drivers benefit from frequent updates of our products to enhance station management and charging experience.

Features not included in the Core plan, but available with plan upgrade:

Driver Access & Payment

  • Time-Based Access Control - Change public access based on the day and time for each location. For example, a location can be available to the public during the day but limited to user groups and access code drivers at night.

           ❌Starter | ❌Core | ✅Pro

  • Session Limits & Idle Fees - Encourage drivers to share charging stations by imposing time limits or charging idle fees for drivers staying after a certain time period. Drivers receive push notifications warning them of the session limit and incurring idle fees. 

         ❌Starter | ❌Core | ✅Pro

Revenue Generation

  • Tiered Pricing - Set two-tier charging rates with one price for an initial time period or energy usage and a different rate thereafter. For example, free for the first hour, and then $2 per hour after; or $0.10/kWh for the first 15 kWh, and then $0.30/kWh after. 

         ❌Starter | ❌Core | ✅Pro

  • Time-of-Use Rates - Manage pricing based on the time of day to accommodate for different utility rates or driver demand. For example, utility electricity prices may increase between 4-9pm and charging pricing rates can be set higher during those times.

          ❌Starter | ❌Core | ✅Pro

Location & Account Management

  • Advanced Load Management - Set an energy load cap that limits the maximum power available across a location to reduce the load on the panel. For example, a location could have twenty charging stations each rated at 7.6kW each (a total load of 152 kW if all twenty stations were used at the same time). If the load cap were set to 76kW, 10 cars could charge at 7.6kW. If eleven cars were to charge, the stations would automatically throttle to 6.9kW (76kW/11 cars). Site hosts should work closely with their electrician to determine the load cap and if this feature is required for their location.

         ❌Starter | ❌Core | ✅Pro

(What is included in the CORE plan? – Support Center)

The AmpUp Starter plan includes:

  • STARTER $175/year:
    • Analytics & Reporting
    •  Driver Reservations
    • Driver RFID Card
    • Location Access Control
    • Driver Support
    • Remote Troubleshooting
    • Standard Host Support
  • CORE $250/year:
    • Everything in STARTER +
    • Revenue Collection
    • Direct Deposit
    • Driver Access Groups
    • Multi-Site Management
    • Multi-User Account
    • Extended Host Support
  • PRO $350/year:
    • Everything in CORE +
    • Tiered Pricing
    • Time-of-Use Rates
    • Time-Based Access Control
    • Session Limits & Idle Fees
    • Advanced Load Management
    • Premium Host Support

** Pricing is as of March 2024 and is subject to change. For the most updated pricing visit:

AmpUp EV Charging Made Simple, Getting Started with AmpUp – Support Center

To lower the charging output of your EV Series Pro charger, you will have to go through the AmpUp dashboard within the AmpUp Pro plan. For notifications and alerts, you can see the EV charging management journey, and they include details of drivers’ charging sessions, while alerts keep track of any changes made in the community manager settings and any hardware issues. This video will show you how to interact with notifications about your chargers and drivers. In terms of setting up software with your EV Series Pro Charger, your contractor or installer is responsible for registering and verifying your chargers with AmpUp as part of the installation process. Once this is complete, you will receive a link to start your account setup. Additionally, EV Series Pro chargers are 4G enabled, and they must be installed in an area with an adequate cellular reception. There are cell signal testers available on the market to test signal strength at any given site.

The EV Series Pro isn’t about innovation, it’s about leading the charge toward a smarter, more sustainable future. Whether you’re learning about its features, configuring your device, or troubleshooting, this blog is built to support you every step of the way. With the future of mobility shifting toward electric, the EV Series Pro is ready.

For more information about the EV Series Pro, visit EV Series Pro – Leviton Electric Vehicle Charging.