USB Receptacles | Safety Devices | Leviton Product Support
Product Information
- Are USB connected devices protected from overcurrent?
- What is Dynamic Power Sharing?
- What is the maximum charging output of the Leviton Dual Type-C with Power Delivery (PD) USB Charger Outlet?
- What standards and regulations do Leviton USB In-Wall Chargers meet?
- What is the Leviton 4-Port USB Charger?
- How do I know if my device is PD-enabled?
- Why would I want the Leviton Dual Type-C with Power Delivery (PD) USB Charger Outlet?
- What is Power Delivery (PD)?
- Is USB 3.1 the same as USB Type-C?
- Is Thunderbolt the same as USB Type-C?
- Can I charge my older devices on the USB Type-C port?
- What is USB Type-C?
- Will Leviton USB In-Wall Chargers work as a data transfer port?
- Can I charge multiple tablets at once?
- How long will it take my electronic device(s) to charge?
- What devices can be charged using Leviton USB In-Wall Chargers?
- What are the electrical ratings for the outlets?
- What is the maximum power capacity of the USB charger ports?
Device Setup and Configuration
- Where can I install a GUAC1 or GUAC2 GFCI combination USB outlet?
- What is an “extra deep wallbox”?
- Can the GUAC1 or GUAC2 USB GFCI receptacle be installed in a standard size wall box?
- How do I know if I need Type A or Type C charging port?
- Will Leviton USB In-Wall Chargers work with older devices?
- Can I install two Leviton USB In-Wall Chargers side-by-side?
- Do Leviton USB In-Wall Chargers fit in a standard wallbox?
Device Wiring
Troubleshooting After Installation