Loading...

Lighting Controls | For Every Home

From Traditional to Smart, and Everything In Between

Leviton makes high-end lighting controls accessible, with a focus on future-forward innovation and performance you can trust. Leviton introduced our first Decora Switch in the early 70’s and has been making best-in-class dimmers at the forefront of changing lighting technology ever since. Leviton dimmers provide a smooth full range dimming experience, employing the latest in dimming technology, features, and proven LED compatibility.

LED Advanced dimming

Leviton Lighting Controls products with the LED Advanced badge are designed to deliver superior, flicker-free dimming performance with modern LED bulbs and fixtures. LED Advanced dimmers provide smooth, consistent light control, expanded LED compatibility, and adjustable settings to fine-tune dimming performance.

Explore Our Lighting Controls Products

Our lighting control’s portfolio offers a wide range of solutions across product families to meet the needs of any room and home.

Never arrive home to a dark house

Create custom schedules in the My Leviton App

EXPLORE DECORA SMART

Controls that work automatically

Hands-free lighting and humidity controls

Before and After Dimming

Experience how smooth, customizable dimming transforms any space from bright energy to effortless ambiance.

placeholder

LED Compatibility Tool

Leviton’s LED Compatibility Tool helps customers quickly identify which LED bulbs have been tested and confirmed to work with Leviton dimmers and lighting

Frequently Asked Questions

Visit Leviton.com/LED to determine dimmer and bulb compatibility.

LED dimmers are designed to work with dimmable LED, dimmable CFL, incandescent and halogen bulbs. Some models will also work with Magnetic Low Voltage (MLV) and Electronic Low Voltage (ELV) loads. Leviton recommends only LED bulbs that are labeled DIMMABLE be used. The packaging on the bulb should identify it as dimmable.

Electronic Low Voltage (ELV) dimmers incorporate reverse-phase dimming control, which tends to provide enhanced performance with dimmable LED bulbs. Before using an ELV dimmer with LED/CFL bulbs, ensure the dimmer indicates that it is listed for use with these bulb types. ELV dimmers require connection to a neutral wire, which is often not available in older construction. In addition, Electronic Low Voltage dimmers are typically a more expensive solution.

Leviton offers dimmers for neutral and no-neutral applications.

The neutral wire is generally white and serves as a “path home” for the additional electricity used to power the dimmer. Some dimmers with higher ratings, or advanced technology, require a neutral wire for operation. Be sure to refer to the dimmer specifications on the packaging to find out if a neutral wire is required.

Single pole means controlling light(s) from one location. 3-way is the ability to control light(s) from two separate locations. Multi-Location or Multi-Way is the ability to control light(s) from 3 or more locations.

We strongly recommend you use the same light source to achieve consistent performance from bulb to bulb. If you choose to mix bulb types on the same dimmer, it is possible that you will experience a variation in dimming performance and start up characteristics.

Resources