Loading...

Is Thunderbolt the same as USB Type-C?

Thunderbolt and USB Type-C (3.1 Gen2) share the same cable type and port. Type-C is the physical shape of the connector, USB 3.1 and Thunderbolt are features embedded in the connector.