Product Information
- Are Dual Function AFCI/GFCI Receptacles tamper-resistant?
- Why would I use an AFCI/GFCI Receptacle instead of breaker?
- Is the “Dual Function” AFCI/GFCI the same as a “Combination” AFCI
- Are Leviton Dual Function AFCI/GFCI Receptacles UL listed?
- Does the self-test (auto-monitoring) feature in the Dual Function AFCI/GFCI Receptacle apply to both the GFCI and AFCI functionality?
- Does every receptacle in my home have to be a Dual Function AFCI/GFCI?
- Why would I need a receptacle that has both AFCI and GFCI protection?