Loading...

Why would I use an AFCI/GFCI Receptacle instead of breaker?

The AFCI/GFCI Receptacle can be a great alternative depending on the circumstance. The AFCI/GFCI Receptacle works with any type of wiring and is not dependent on the type of breaker in the panel. It is also easily accessible and has a level of familiarity with users with the TEST and RESET buttons that are also present on a GFCI receptacle.