Loading...

Does every receptacle in my home have to be a Dual Function AFCI/GFCI?

No. The latest National Electrical Code requires both AFCI and GFCI protection only in kitchens and laundry rooms. And within those rooms, the Dual Function AFCI/GFCI Receptacle provides what is called “feed-through” protection, which means it provides protection for all wiring and extensions attached to the load side. If the Dual Function AFCI/GFCI replaces the first receptacle in the branch circuit, it
will provide protection to the remaining outlets on that circuit.