Loading...

Why would I need a receptacle that has both AFCI and GFCI protection?

In 2014, the National Electrical Code® (NEC®) introduced AFCI requirements for kitchens and laundry rooms. The code had previously required that these locations needed only GFCI protection, but for added safety, they are now required to have both AFCI and GFCI protection. Additionally, there has long been a requirement for adding GFCI protection when replacing non-grounding type receptacles. Newer requirements include adding AFCI protection when replacing receptacles in various locations such as living rooms and bedrooms. The Dual Function AFCI/GFCI Receptacle provides an ideal solution for replacing receptacles in these circumstances.