Loading...

Can the same neutral wire be used for the installation of more than one Dual Function AFCI/GFCI Receptacle?

While Dual Function AFCI/GFCI Receptacles can work with a shared neutral on the line side, please refer to specific code requirements regarding acceptable methods for feeding an AFCI/GFCI receptacle. If you are unfamiliar with the function of a neutral wire, contact an electrician.