Loading...

Certificates and Policies

Tender Support | Italy

UK Certificates

Royal Society for the Prevention of Accidents (RoSPA) In 2024, we received our 7th consecutive Gold Award which is the highest available. The award requires a very detailed, evidence based, submission covering all aspects of Health, Safety, and Welfare that includes accident statistics, accident prevention strategies, risk assessment etc. across 19 categories.

RoSPA Gold Award is comparable with ISO 18001, if not more difficult to achieve, on an on-going basis due to the detail of the submission.