Loading...

Do Sensors Require a Ground Connection?

Some Leviton sensors require a ground connection for operation. Leviton’s new line of sensors have flexible wiring options with a wire that can be connected to a neutral or a ground connection. For these sensors, it is recommended to only connect to the ground if there is not a neutral wire present in the wallbox. See below for ground/neutral requirements for Leviton sensors:

 

Product

Ground Required?

Neutral Required?

IPS02/IPV02

Yes

No

IPS05/IPV05

Yes

No

IPS06

Yes

No

IPSD6/IPVD6

Yes

No

IPS15/IPV15

No

Yes

IPHS5

No

Yes

DOS02/DVS02

Either Neutral or Ground Required

Either Neutral or Ground Required

DOS05/DVS05

Either Neutral or Ground Required

Either Neutral or Ground Required

ODS10

Yes

No