Loading...

Leviton Expands Portfolio of Outdoor Copper Cable Assemblies

New stocked solutions meet growing demand for exterior network device connectivity, help simplify network connections for outdoor Ethernet applications 

News Summary

  • Expanded Outdoor Connectivity Portfolio: Leviton has introduced a line of stocked Outdoor Copper Cable Assemblies, including Cat 6A, Cat 6 and VXC assemblies, to support the increasing deployment of exterior network devices like security cameras, access control and IoT sensors.
  • Support for Deployment of Outdoor Connected Devices: Designed for applications like commercial buildings, campuses, schools, healthcare facilities, industrial sites and public spaces where the number of IP-enabled devices installed outdoors continues to increase.
  • Engineered for Harsh Outdoor Environments: Built with compact, moisture- and UV-resistant black jackets, these assemblies comply with ANSI-TIA-568.2 and ISO/IEC 11801 standards to ensure reliable network performance against outdoor exposure.

Bothell, WA, October 20, 2026 — Leviton, a global leader in electrical, lighting and networking systems, today announced an expanded line of stocked Outdoor Copper Cable Assemblies designed specifically to support organizations working to expand deployment of connected devices beyond the walls of the building.

Enabling a large range of applications, our stocked line of Outdoor Copper Cable Assemblies includes:

Across commercial buildings, campuses, schools, healthcare facilities, industrial sites and public spaces, the number of IP-enabled devices installed outdoors continues to increase. Perimeter security cameras, thermal imaging systems, integrated security solutions, access control points and other intelligent devices are critical components of the modern network infrastructure. 

Connecting these devices often requires portions of the network cabling to be exposed to sunlight, moisture and other environmental conditions. Leviton’s new Outdoor Copper Cabling Assemblies are designed to address this growing challenge while helping simplify installation and maintain reliable network performance.

"More of today's network-connected devices are being installed on the exterior of buildings than ever before," said Kirk Krahn, Director of Product Management for Leviton Network Solutions. "Whether supporting cameras protecting a facility, access control systems securing entrances or specialized IoT devices monitoring the environment, contractors and installers need connected solutions designed for outdoor exposure. These new Outdoor Cable Assemblies provide a straightforward way to extend network connectivity to those devices while leveraging the performance and reliability customers expect from Leviton."

Key product features include:

  • Cable jacket construction providing Moisture- and UV-resistance for outdoor applications
  • Compact cable diameter of 0.25 inches (6.35 mm) or less for easier routing
  • ANSI-TIA-568.2 and ISO/IEC 11801 performance compliance
  • Black-jacket construction optimized for outdoor environments
  • Availability in configurations with additional custom lengths available upon request

"These new cable assemblies build on our recent extended distance solutions, enabling customers to address increasingly demanding edge-network deployments while maintaining a standards-based architecture," said Krahn.

Leviton Outdoor Copper Cable Assemblies are assembled in the United States for responsive service and fast turnaround.

For more information about Leviton's Outdoor Copper Cable Assemblies and the company's complete portfolio of copper and fiber connectivity systems, visit https://leviton.com/ns. 

Frequently Asked Questions

Q: What environments and applications are these outdoor cable assemblies designed for?
A: Leviton Outdoor Copper Cable Assemblies are built for commercial, campus, healthcare, industrial and public environments. Featuring moisture- and UV-resistant jackets, they connect exterior IP-enabled devices such as perimeter security cameras, entrance access controls, thermal imaging systems and outdoor IoT sensors.

Q: What cable options and lengths are available?
A: The stocked lineup includes a 20-foot Cat 6A Outdoor Patch Cord, a 25-foot Cat 6 Outdoor Patch Cord and a 15-foot VXC Assembly with RDT I/O cable that connects without punchdown tools. Custom lengths are also available upon request.

Q: Where are these assemblies manufactured, and what standards do they meet?
A: Assembled in the United States for fast turnaround, the cable assemblies feature a compact cable diameter of 0.25 inches or less and comply with ANSI-TIA-568.2 and ISO/IEC 11801 performance standards.

__________________

About Leviton Network Solutions
Leviton Network Solutions is a single-source, carbon neutral manufacturer of global end-to-end copper and fiber cabling systems. Deployed in data centers, smart buildings, and harsh environments around the world, our global systems are engineered to exacting standards and are available globally through our extensive distribution network. Leviton Network Solutions delivers value by providing speedy service, scalable solutions, assured performance, and an agile collaborative process. Leviton was established in 1906 and continues to invest in and grow our business. Together, let’s build what’s next for your network.  Learn more at www.leviton.com/ns or linkedin.com/showcase/levitonns. European customers can visit leviton.com/ns/emea or linkedin.com/company/Leviton-ns-eu.