Loading...

How to Wire a Device Using the Quickwire Method

YouTube Video

"Quickwire” type of termination is found on residential grade switches and receptacles. “Quick wire” is also known as “speedwiring"",“stabbing” or “back stab” termination.

To quickwire a switch, first use the backwire push-in feature (also referred to as "backstab")

Next, Insert the wire directly into the Quickwire hold on the back of the device. The Quickwire hole ONLY accepts 14 gauge solid wire. See image diagram below.

Additionally, watch this Leviton video to learn how to wire a device using this method.

If you're ever unsure about wiring a device, please consult an electrician. For more information on specific termination methods or wiring of Leviton devices, visit Leviton.com

Quickwire