Loading...

Preventing Electrical Shocks with GFCI Outlets

Electrical shock is often caused by ground faults, which occur when electricity flows along an unintended path—such as through water, damaged wiring, or a person. These conditions commonly arise when electrical devices are used in wet or damp environments, where electricity and moisture can come into contact.

GFCI (Ground Fault Circuit Interrupter) outlets are designed to reduce the risk of electrical shock. They continuously monitor the flow of electricity and, if a ground fault is detected, automatically shut off power in a fraction of a second. This quick response helps prevent serious injury and can save lives.

Ground faults may be caused by:

  • Using electrical equipment near water
  • Damaged or frayed appliance cords
  • Electrical current leaking from tools or appliances

GFCI protection is especially important in areas of the home near water, which is why the National Electrical Code (NEC) requires GFCI outlets in locations such as kitchens, bathrooms, and other damp areas.

Leviton offers a wide range of GFCI options to meet different needs, including tamper‑resistant, weather‑resistant, guide‑light, audible, and blank‑face models. Choosing the right GFCI outlet helps provide essential protection against electrical shock while meeting code requirements.

For more information about GFCI outlets and electrical safety, visit Leviton.com/GFCI.

YouTube Video