Loading...

The Difference Between GFCI Breakers and GFCI Outlets

Have you ever wondered how to choose between circuit breaker and outlet protection? Watch this video to learn the benefits of both. To learn more about GFCIs, visit: http://leviton.com/gfci

This video explains the key differences between GFCI outlets and GFCI circuit breakers and how each provides ground‑fault protection required by the National Electrical Code in areas near water, such as kitchens, bathrooms, pools, and spas. GFCIs help prevent electrical shock by detecting ground faults and shutting off power.

GFCI outlets protect the outlet they are installed in, as well as any downstream outlets on the same circuit. They offer convenient, point‑of‑use testing and resetting directly at the receptacle, with indicator lights showing operating status.

GFCI circuit breakers are installed at the electrical panel and protect an entire circuit from a single location. They are typically used for applications with larger electrical loads, such as spas or hot tubs, since they are available in higher amperage ratings. GFCI circuit breakers also include visual status indicators to quickly show whether protection is active or if the breaker has tripped.

Both options provide essential protection, but the best choice depends on the application, load requirements, and installation preferences.

YouTube Video