Loading...

I have an LDATA and changed my Wi-Fi, how do I update my LDATA Wi-Fi settings?

If you are installing a new Wi-Fi network with the same SSID (network name) and password your LDATA will use the new network after a restart.  If you are changing the SSID or password you can follow the following procedure to update Wi-Fi credentials without defaulting the LDATA or repeating the breaker pairing process.

To update your LDATA Wi-Fi settings without resetting your LDATA you must first restart (power cycle) your LDATA and the original Wi-Fi network must not be available.  Your mobile device running the My Leviton app must have access to the My Leviton cloud connected to a different Wi-Fi network or connect using a cell data connection.

When the LDATA is rebooted without the Wi-Fi network available the My Leviton app will show the Load Center as offline:

LDATA

The instructions offer options to get back on-line if the credentials have not changed.  Since the credentials have changed, please ignore this option and press the back < icon in the upper left corner.

LDATA

Choose settings

LDATA

Choose Leviton Load Center Options

LDATA

New options will be available from the bottom of the screen.  Choose Change Wi-Fi Network.

LDATA

Choose Go to my Wi-Fi settings

LDATA

Your LDATA must be booted without access to the Wi-Fi network.  Note, the LDATA can take up to 5 minutes to boot.  Choose the LDATA-**** in the Wi-Fi Network.

LDATA

Follow the enrollment process found in the article Adding a Leviton Smart Load Center.

Note: the LDATA will scan for breakers and previously paired breakers do not need to be reconfigured.