Loading...

If I Have Multiple Decora Smart® Wi-Fi Bridges (MLWSB) How Do I Connect To The Bridge With The Best Signal?

For installations that require multiple MLWSB Decora Smart Wi-Fi Bridges, you will need to enroll the bridges into your My Leviton account prior to adding the DN No-Neutral switches and dimmers. See the article How Many Devices Can I Connect To A MLWSB And What Is The Wireless Coverage Area?  If you are adding new DN No-Neutral devices you may want to update an existing connection to improve performance. 

  • Add all MLWSB Decora Smart Wi-Fi Bridges using the article Add a Decora Smart® No-Neutral Device to the My Leviton App
  • If you have a previously installed DN device that may benefit from a newly added MLWSB Decora Smart Wi-Fi Bridge, use the Reconfigure Wireless procedure  
    • Press the 3 Dots in the upper corner of the DN Dimmer or Switch
No Neutral
  • Choose Device Settings
No Neutral
  • Choose Reconfigure Wireless
No Neutral
    • Place the DN Switch or Dimmer into setup mode by pressing and holding the top rocker
      • After 7 seconds the bottom LED will turn amber
      • Let go of the rocker
      • The bottom LED will flash green
    • Follow the in-app instructions
      • Note, your device icon, name and room location will all be remembered when you update the wireless connection