Loading...

How many devices can I connect to a MLWSB and what is the wireless coverage area?

The MLWSB Decora Smart Wi-Fi Bridge provides up to 2,500 sq. ft. of coverage, and should be placed in a central location within 50 ft. of Decora Smart No-Neutral devices.  One Decora Smart Wi-Fi Bridge supports up to 25 devices.  Multiple Bridges can be installed per residence to provide increased coverage in larger homes.

NOTE: One MLWSB Decora Smart Wi-Fi Bridge supports up to 6 Anywhere Companions paired to associated Decora Smart No-Neutral devices.