Loading...

What Copper Cable is Best for PoE Applications?

A Guide to Selecting Enterprise PoE Solutions and Managing Temperature Rise

When Power over Ethernet (PoE) was introduced in 2003, it was available for only a handful of low-power operations and devices. Today, PoE is one of the fastest growing networking applications, and it is on the rise due to the wide range of benefits it provides, including: 

  • Lower cost compared to a line voltage system and a separate network for data
  • Improved system control
  • Greater operational efficiency
  • Opportunities for technology expansion
  • Network future-proofing

A wide range of enterprise devices and technology rely on PoE, including lighting, access controls, IP cameras, information kiosks, industrial automation equipment, and wireless access points (WAPs). With the advent of the Internet of Things (IoT) and digital buildings, PoE is poised for unprecedented expansion in the enterprise. 



The PoE market has flourished and is projected to continue its rise through 2030, indicating a continuing demand for PoE capabilities in the enterprise.

 

What copper cable provides the best value for PoE applications, now and in the future? It won't surprise you that there isn't a "one-size-fits-all" answer; network architecture resists templatization, and so different copper cables will provide a better value in specific situations. However, a good rule of thumb is to choose a copper cable that can perform at the level of power needed without exceeding its maximum temperature.

What we aim to do with this article is equip you with the knowledge to choose the copper cable that will provide the best value for your network architecture, examining the varying characteristics of PoE copper cabling and the impact they have on temperature rise to help you  identify the solution you need.

Managing Temperature Rise

When twisted-pair cabling is used for PoE, the majority of the power entering the cable is successfully delivered to the device being powered. However, a small percentage is dissipated in the cabling as heat. This can cause the cable’s temperature to increase above the temperature of its surroundings.

The maximum temperature to which a cable will increase depends on a number of factors, including:

  • The amount of power being applied to the cable
  • The cable's resistance/construction
  • The number of cables in a bundle laid in tray

It's critically important at higher levels of PoE to keep temperatures below the cable's maximum limit, as this will prevent transmission impairment due to structural compromise and reduce long term cable degradation. We’ll take a quick look at three key factors, conductor size, bundle size, and shielded or unshielded cable constructions, and how they can have a major impact on temperature rise within PoE cabling.

Conductor Size

Conductor size plays an important role in PoE performance because electrical resistance increases as conductor size decreases. Larger conductors have lower DC resistance, which helps deliver power more efficiently and reduces heat buildup within the cable. As PoE power levels continue to rise, minimizing cable heating becomes increasingly important for maintaining long-term network performance and reliability.

Conductor size factors into:

  • Improving efficiency: Larger conductors reduce DC resistance, helping more of the supplied power reach connected devices instead of being dissipated in the cabling
  • Reducing heat: Lower-resistance conductors help minimize temperature rise within cable bundles, an important consideration as PoE power levels increase
  • Enhancing reliability: Better power delivery and lower operating temperatures help maintain consistent network performance over time

 



Larger conductors will heat up less and perform better than smaller conductors.

Bundle Size

If cables are bundled or closely grouped with other cables, cables near the center of the bundle have difficulty radiating heat out into the environment. Therefore, the cables in the middle of the bundle heat up more than those toward the outer layers of the bundle. The larger the bundle size, the more the cables in the center will heat up.

To minimize the effect of bundle sizes on temperature rise, try:

  • Separating large cable bundles into smaller bundles or avoiding tight bundles will reduce temperature rise.
  • Where possible, plan the rack layout for non-powered and powered cables to be mixed in the same bundle, and place non-energized cables in the center of the bundle and energized cable in the outer layers of the bundles.


Loosely group cables when possible, rather than bundling. If bundling is required, loosely bundle cables in the smallest bundle size that suits the needs of the installation.

Shielded or Unshielded Constructions

You may also consider using a shielded cabling system, or unshielded (UTP) cables with a metallic isolation wrap. These cables radiate heat better than traditional UTP cable, minimizing the cables' temperature rise.

Leviton engineers recently tested how cable construction affected temperature rise. They compared three cable types: traditional Unshielded Twisted Pair (UTP) cable; UTP cable with a Leviton patented metallic "isolation wrap" that surrounds the 4-pair core; and shielded (F/UTP) cable. This design provides additional alien crosstalk suppression while eliminating the need for grounding and bonding typically required with shielded cabling.

Testing these cable types in 37-cable bundles found:

  • Both shielded and isolation-wrap cable performed better than traditional UTP cable
  • The average temperature rise within the shielded cable bundle was more than 2°C lower compared to the traditional UTP cable bundle.

 


Rigorous testing in the Leviton labs illustrated a clear difference in temperature rise between traditional UTP cable and shielded varieties.

Choosing the Right Copper PoE Cable

High-quality connectivity is essential for attaining the performance and reliability needed in current and future PoE network operations. System components should be designed to minimize temperature increases and meet industry standards for performance and construction. This ensures system longevity and prepares networks for future upgrades and growth.

Leviton systems for PoE — including cable, connectors, patch cords, and patch panels — are component rated, and third-party tested and verified to exceed industry standard performance. Leviton ATLAS-X1™ Cat 6A connectivity and SST Cat 6A UTP Cable are tested to deliver 100-watt PoE, enabling the transmission of power and data to a wider range of remote devices. System components have undergone rigorous lab testing to meet the need for higher bandwidth and power, while limiting the temperature rise in large cable bundles and remaining within the cable’s listed rating.

For more on Leviton’s PoE copper systems, visit our PoE page.