Loading...

Dimmer Switches

Adjust Your Lighting for Any Activity

Open concept living room and kitchen
Replacing a wall light switch with a dimmer switch is an easy way to create a big impact for a minimal cost. Using a dimmer switch makes it easy to customize the light level in any room, for any occasion and in any home. Leviton has a large selection of dimmers in different styles and types so you can choose what best meets your needs – traditional, decorator, or smart. They are all designed to control any bulb type including a full selection of dimmers specifically for LED lights.

Why Replace a Wall Switch with a Dimmer Switch?

Explore our Dimmer Switches

Key Features of Leviton Dimmers

Superior Performance

Leviton LED dimmers feature a mode selector switch to modify the minimum and maximum light levels, if needed, for optimal performance every time.

placeholder
Changeable Faceplates

Removeable faceplates on select models allow users to easily change the color of the device by removing the faceplate and snapping on a new color.

placeholder
Preset Lighting

Separate dim/bright adjustment to preserve set light level is standard on many models.

placeholder
Single Pole or 3-Way Control

Many Leviton dimmers offer the flexibility of control from one or more locations. Ideal for great rooms with multiple entrances, or for placement at the top and bottom of a staircase.

placeholder

What Type of Dimmer Switch Do You Need?

The dimmer switch you need is based on the application and how many lights you are controlling. Download this infographic.

Single-Pole Application

Dim the light(s) from one location using a single dimmer switch.

placeholder
3-Way Application

Dim the light(s) from one location using a dimmer switch and a 3-way light switch from a second location to turn the light(s) on and off.

placeholder
Multi-Location (Multi-Way) Application

Dim the light(s) from 3 or more locations using a dimmer switch and dimmer companions.

placeholder

Decora Smart® Dimmer Switches

Smart home lighting you can control from anywhere

  • Use the My Leviton app, a time schedule, or your voice to set the scene and manage  lights, electronics, and small appliances with Decora Smart Wi-Fi devices. You can start small with a smart switch to control your porch light or go BIG and outfit your entire home. Decora Smart Wi-Fi is customizable to meet your specific needs.
Learn more
placeholder
placeholder

Decora Dimmer Switches

Great design stands the test of time

  • Our Decora brand has set the industry standard for style and performance. Our robust collection of digital and slide dimmers offers contemporary elegance and adds a finishing touch to any room. 
Decora Digital™ Dimmers  Decora Slide® Dimmers 
Decora Lever Edge Dimmer IllumaTech® Dimmers  SureSlide® Dimmers

Traditional

Classic look with modern performance

  • For traditional homes, our Toggle and Rotary style dimmers offer the ideal way to upgrade functionality and support the latest bulb technology without compromising the character of the décor. 
Toggle Dimmers  Rotary Dimmers
placeholder
placeholder

Tabletop and Specialty Dimmers

Stylish solutions that make dimming easy and convenient


Blogs

Videos

YouTube Video
Leviton Answer Series: All about Dimmers

Learn the ins and outs of Leviton dimmers.

YouTube Video
Leviton Answer Series: Single Pole vs. 3-way Controls

Learn about the differences between a single pole and 3-way control.

YouTube Video
How to Avoid LED Bulb Flicker

Avoid the flickering lights and let Leviton help you find the perfect dimmer switch and LED bulb combination.

Find a Compatible LED Bulb

Dimmer and bulb compatibility are important for great lighting. Use our LED Bulb Compatibility Selector Tool to find the perfect match for your Leviton dimmer! It’s available online or on the go using the Leviton2Go mobile app.

Dimmer Frequently Asked Questions

Additional support can be found on our Dimmer product support hub

Not all LED bulbs dim smoothly with every Leviton dimmer. Use the Leviton Dimmer and LED Compatibility tool to find a compatible bulb and dimmer pairing.

A switch that allows you to dim a light from one location using a dimmer switch, while a 3-way switch at a second location can turn the lights on and off.

Generally, halogen bulbs are dimmable when used with a compatible dimmer.

 

Dimmer switches let you customize light levels for different activities, reduce energy consumption, and help optimize the performance of compatible lighting.

Yes, Leviton offers dimmers designed to work with existing wiring 

A dimmer offers more control over light output than a switch, allowing the user to fine-tune the lighting in their space.

Yes, dimmed lights use less energy, which can help reduce electricity costs.

Some dimmers contain a metal mounting strap that has fins designed to dissipate heat from the device. If more than one dimmer is being installed in a multi-gang application, the user may be required to break off the fins before installing. Please refer to installation instructions for when it is necessary to remove the fins.

Derating may be required if you have two or more dimmers sharing a wallbox to help dissipate the internal heat of the dimmer. Some dimmers will have fins (heat sink) on the side which will need to be removed. This   decreases the wattage capacity that the dimmer can control. Be sure to refer to the dimmer instruction sheet for fin removal. Derating is NOT required when using dimmable LED or dimmable CFL bulbs. Refer to the derating chart in the instructions for maximum load per dimmer.

Leviton dimmer switches put you in control

Set the mood by adjusting the light level for any activity. Whether you are entertaining, reading, keeping the little ones safe from bedtime “monsters” or watching the latest flick, the right lighting creates the perfect ambiance. Use our Dimmer Buying Guide to find the best dimmer for any room in your home.

 

DOWNLOAD GUIDE

family on sofa

Resources


How Can We Help?

Do you have questions about our dimmers?