Glenrothes, UK, January 7, 2025 – Leviton is excited to announce the launch of two ADVENTUM™ Central Dry Tube cables: Fire Survival and RailSafe Steel Tape Armor. These cables prioritize safety, delivering exceptional fire performance, top-tier efficiency, and a robust return on infrastructure investment for where low smoke or CPR requirements are specified.
ADVENTUM™ Fire Survival is an indoor cable, engineered to ensure critical data transmission during fire emergencies. Meeting the rigorous flammability standards of IEC60331-25, these cables can maintain circuit integrity for 90 minutes (PH90 – EN50200) under extreme conditions, making them indispensable for large public buildings and crucial infrastructure. Meanwhile, ADVENTUM™ RailSafe cables adhere to comprehensive standards, including the London Underground’s LUL S-1085 specification, ensuring they are perfectly suited for underground rail networks, stations, tunnels, and tracksides.
Both cables are manufactured in Leviton’s UK cable factory and form part of the continued expansion of the ADVENTUM™ family, boasting some of the brand’s key advantages. In this case, the Central Dry Tube cuts the time-consuming mess of wet gel constructions, whilst the added incorporation of high-strength, corrugated Steel Tape Armor provides exceptional defense against external factors, whether they be mechanical impact, rodent damage, or environmental elements.
“All of this represents Leviton’s proud investment in the ADVENTUM™ brand, an acknowledgement of its key advantages in meeting evolving installation needs,” states Michael Lawrence, Product Manager at Leviton Network Solutions Europe. “This acknowledgment also led us to question how we might bring greater value to our customers, which is why we have now enhanced our existing Central Dry Tube, Non-Armored cable with ADVENTUM™ water-blocking technology.
“With exciting innovations on the horizon, we look forward to delivering more ADVENTUM™ advancements, all manufactured using 100% renewable energy in our UK-based, carbon-neutral facility.”
For more information, visit leviton.com/adventum.
__________________
About Leviton Network Solutions
Leviton Network Solutions is a single-source global manufacturer of copper and fiber cabling systems. Leviton solutions are used in data centers, businesses, schools, hospitals, government facilities and commercial mixed-use markets around the world. All Leviton products are engineered to exacting standards, offer industry-leading performance and are backed by the industry's best service and support. IT management, builders, contractors, and other industry professionals consistently rank Leviton products as the most preferred brand in the industry. We can expand your network possibilities. Learn more at www.leviton.com/ns or www.twitter.com/LevitonNS. European customers can visit leviton.com/ns/emea or twitter.com/LevitonNS_EU.