Yes, models with higher ratings such as the DOS05, DVS05, IPS15 and IPV15 are designed to control exhaust fans.
Product Bulletin
Decora Occupancy Motion Sensor Light Switch | DOS05, DVS05 | EN
Decora Occupancy Motion Sensor Light Switch | DOS05, DVS05 | FR
Decora Occupancy Motion Sensor Light Switch | DOS05, DVS05 | ES
Leviton L-400 Full-Line Catalogue
Instruction Sheet - Decora | Decora Motion Sensor In-Wall Switch | IPS15, IPV15 | EN
Instruction Sheet - Decora | Decora Motion Sensor In-Wall Switch | IPS15, IPV15 | FR
Instruction Sheet - Decora | Decora Motion Sensor In-Wall Switch | IPS15, IPV15 | ES
Additional FAQ's