Dimmers that dissipate current from a source are current sink type and are commonly used in commercial and residential applications. In this scenario, the ballast/driver is “sourcing” the current and the dimmer is “sinking” the current. The ballast/driver is providing the source of power and the dimmer is providing the dimming signal between 0-10V.
What is the Difference Between Sinking and Sourcing?