Loading...

What to do when your GFCI outlet trips?

Your GFCI outlet tripped...now what? This video explains what to do when a GFCI receptacle trips and when it may be time to call an electrician. GFCIs are important safety devices that protect against electrical shock by shutting off power when a ground fault is detected, such as current flowing through water or a person. Even with built‑in self‑testing features, GFCIs should be visually inspected and tested monthly.

If a GFCI trips, begin by checking the outlet for visible damage such as discoloration or loose connections. If damage is present, the outlet should be replaced. If the GFCI appears to be in good condition, consider what was happening at the time of the trip—such as plugging in or using a specific appliance. Inspect any connected appliances, cords, and downstream outlets for signs of damage or wear. A faulty device may be causing the GFCI to trip and should be unplugged.

If the GFCI continues to trip or there is no obvious cause, contact a qualified electrician to inspect the circuit. Safety should always be the top priority.

YouTube Video