Loading...

GFCI Line/Load Reversal

This video explains how to properly install a GFCI receptacle and avoid a common wiring mistake called line‑load reversal. The line wires bring power from your home’s electrical panel to the GFCI, while the load wires carry power from the GFCI to other outlets downstream. Each set of wires must be connected to the correct terminals on the device.

If the line and load wires are mixed up, the GFCI will not provide proper protection. Leviton Smartlock Pro GFCIs include a built‑in safety feature that prevents power from turning on if this wiring mistake occurs. Fortunately, the fix is simple—rewiring the GFCI correctly will restore normal operation. 

Helpful Tips

  • Always follow the installation instructions and diagrams included with your GFCI receptacle.
  • Leviton provides step‑by‑step GFCI installation videos and additional support at Leviton.com.
YouTube Video