Loading...

Which Smart Breakers Are Compatible With the LDATA and LWHEM?

In late 2023 Leviton released the Leviton Whole Home Energy Manager (LWHEM) as a replacement for the LDATA.  At the same time 2nd Gen Smart Breakers With On/Off Control were released to add additional control to the Smart Breaker Line.  While attempts were made to offer the widest possible compatibility, not all Smart equipment is interoperable.

Compatibility:

  • LWHEM supports both 1st and 2nd Gen Smart Breakers
  • LDATA is only compatible with 1st Gen Breakers
  • LSBMA CTs are compatible with LWHEM and LDATA
  • LSMMA CTs are only compatible with the LWHEM