Loading...

Can Leviton Load Center breakers be remotely turned on and off?

Leviton has two generations of Smart Breakers:

  • 2nd Gen Smart Circuit Breakers with Remote Control were released in August of 2023 and feature the ability to turn circuits on and off remotely.  These breakers are only compatible with the Leviton Whole Home Energy Monitor (LWHEM) interface.
  • Prior to the 2nd Gen Breakers release, 1st Gen Smart Breakers could be remotely tripped; however, breakers could not be turned back on. 
    • 1st Gen Smart Breakers are compatible with both the LWHEM and LDATA.