Loading...

How Do I Return My Decora Smart® Wi-Fi Device to Factory Default?

Factory defaulting a Decora Smart Wi-Fi device will remove all Wi-Fi information, app setup, schedules and configuration.  It will return to factory settings.  If the device is currently registered it should be removed from the app.

To reset a plugin or outlet to factory settings:
1. Hold the button for a total of 14 seconds.
2. After the first 7 seconds the status light turns amber. Continue to hold.
3. After a total of 14 seconds, the status light will quickly flash red/amber.
4. Release the button and it will reset.

To reset a dimmer,  switch, or fan controller (not including the DWVAA) to factory settings:
1. Hold the top of the rocker for a total of 14 seconds.
2. After the first 7 seconds the status light turns amber. Continue to hold.
3. After a total of 14 seconds, the status light will quickly flash red/amber.
4. Release the top of the rocker and it will reset.

To reset the DWVAA to factory settings requires two different button sequences in order:
First Sequence:
1. Hold the ON and OFF button together for 7 seconds.
2. Release when the status light starts flashing green.
Second Sequence:
3. Press and hold the ON button for 7 seconds, the status light will flashes red/amber
4. Release the top of the rocker and it will reset.

To reset a 4 Button Controller to factory settings:
1. Hold the top button for a total of 14 seconds.
2. After the first 7 seconds the bottom LED turns amber. Continue to hold.
3. After a total of 14 seconds, the bottom button's status light will quickly flash red/amber.
4. Release the top button and it will reset.