On the importance of cabling in AI networks:
McDowell: "Cabling really is the foundation of the data center. There are, of course, a range of important components that make up modern operations, but it’s all too easy to overlook cabling. The reality is, the speed, reliability, and overall performance of the network are only as strong as the cables it's built upon."
On the difference between cabling for AI networks vs traditional data center networks:
McDowell: “AI networks are a completely different beast. And we’re all still learning the best ways to manage them. The nature of these workloads is driving higher densities, more fiber connections per rack, and much greater bandwidth requirements. And this shift is challenging cooling capabilities at the physical layer since clusters packed full of GPUs run hot. Aligning key elements such as cooling with cabling setups is now mission critical – and it requires a lot more forethought. Cabling designed for AI-ready operations has now become what we view as a strategic enabler of performance, and not just a supporting component, as it was often viewed as in data centers of the past.”
On the need for data center operators to use modular structured cabling solutions that will scale and adapt as the technology evolves:
McDowell: “As densities increase, you still need to be able to add or replace individual fibers and cables without disrupting live connections in a production environment. That’s why future-proof solutions are so critical, and low loss, flexible designs built on modular foundations are key differentiators. Each and every one of our systems are engineered to handle these requirements, ensuring networks built for today's needs can handle tomorrow's performance, without a complete architectural overhaul. Our STRATA™ family of solutions is focused on pre-terminated fiber assemblies, very small form factor connectors – whether it’s multi-fiber mating connectors (MMC), multi-fiber push-ons (MPO) or a splicing option – and high fiber count trunk cabling, modularized to provide in-built flexibility and speed up time to market.”
For more of Brad McDowell’s insights on modular solutions, tailoring infrastructure to customer needs, and the next generation of fiber, check out Data Center Dynamics’ article here.