Loading...

Humidity Sensor and Fan Control

Leviton Humidity Sensor and Fan Control in Bathroom

A little heat and humidity is okay for a day at the beach but not so much for inside our homes.  Think damp, humid bathrooms, basements and home spas and the condensation that goes along with it.  Since opening a window just doesn’t cut it, may we suggest the new Leviton Humidity Sensor and Fan Control. This handy sensor automatically detects excess humidity in a room and activates the ventilation fan to lessen condensation which helps to reduce the dreaded mold and mildew.

Imagine how great it would be for the bathroom ventilation fan to automatically switch on as soon as excess humidity is detected during a shower.  The air would become clearer, the dampness and “mirror sweat” significantly reduced and the environment would be so much more comfortable. And, since the sensor is automatic, it will keep the fan running until humidity levels drop to the level you set.  No running back to check on the fan and no more forgetting about the fan and leaving it running for hours on end. Yes, this device is an energy saver as well!

Leviton Humidity Sensor and Fan Control Product

As for the damp, occasionally musty basement, the Air Cycle mode is ideal!  The Humidity Sensor and Fan Control can be set to turn on a ventilation fan for a set period of time and repeat the cycle hourly: for example, 20 minutes ON and 40 minutes OFF every hour. How smart is that?!

Oh, did we forget to mention that it is compatible with incandescent, LED, CFL and fluorescent lighting loads? This handy device can replace a single pole switch, can be used with most bathroom or ventilation fans and offers a flexible installation option, wiring to a neutral wire or to the ground connection. The super slim profile makes installation easier, even in older homes with smaller wallboxes.  You can choose from white, ivory or light almond, and if those colors don’t suit your needs color faceplates are available in white, ivory, light almond, gray, black and brown.

Check out our video below and watch as condensation disappears… visit our Humidity Sensors and Fan Controls page to learn more.

YouTube Video