Loading...

How to Reset a GFCI Outlet After Lockout: A Step-by-Step Guide

GFCI Outlet on Bathroom Wall

If your GFCI outlet refuses to reset, you're not alone. It's a common issue that can be frustrating, especially when first installing the device or when restoring power to a bathroom, kitchen, garage, or outdoor outlet. The good news is that this problem often comes down to a built-in safety feature called Reset Lockout. Understanding how it works can help you address the issue safely.

This blog breaks down what reset lockout is, why it happens, and how to get your GFCI outlet protecting you again.

What is Reset Lockout?

Modern GFCI outlets (Ground Fault Circuit Interrupters) are designed to protect you from electrical shock. They constantly monitor the flow of electricity and trip when they detect an imbalance that could lead to a shock hazard.

The reset lockout feature adds another layer of protection by blocking an outlet from resetting when conditions are not safe. Essentially, the outlet is telling you:

"Something's wrong, and I won't turn back on until the problem is fixed."

This prevents power from being restored to a circuit that could still be hazardous.

Leviton GFCI Outlet

Why Your GFCI Will Not Reset

A GFCI outlet may enter Reset Lockout for several reasons. Some of the most common include:

1. No Power to the Outlet

If the circuit breaker has tripped or there's a loose connection upstream, the GFCI won't reset because it isn't receiving power.

2. A Ground Fault Is Still Present

If the outlet detects a continuing imbalance in the electrical flow, it will stay locked out to prevent shock.

3. Incorrect Wiring

Newly installed or recently replaced outlets may be wired incorrectly. GFCIs will not reset if line and load wires are reversed. 

4. The Outlet Is Damaged

Age, moisture, or internal failure can cause the GFCI to malfunction and refuse to reset.


How to Reset a GFCI Outlet After Lockout

Follow these steps to safely troubleshoot and restore power

Step 1: Check for Power

  • Go to your electrical panel and look for any tripped breakers
  • Reset any that are off or partially tripped
  • Return to the outlet and try pressing the RESET button again

Step 2: Inspect for Ground Faults

  • Unplug anything connected to the GFCI or any outlets downstream
  • Press RESET again
  • If it resets now, one of the devices was causing the fault

Step 3: Test the Outlet

  • Press the TEST button
  • The outlet should click and turn off
  • Press RESET again
  • If it won't reset, the outlet may still be detecting a problem

Step 4: Check for Wiring Issues

If the outlet was recently installed or replaced, incorrect wiring is a likely culprit. Line/load reversal is a common wiring mistake that happens when the line connectors are accidentally connected to the load terminals. To fix this, you would turn off power to the outlet, then disconnect the conductors to swap them before restoring power.

Once corrected, press the RESET button and the GFCI should operate as designed. Always follow the provided instructions and videos, unless you are experienced and comfortable with electrical work this step should be handled by a licensed electrician.

Correct Load and Line Wiring
Leviton GFCI Outlet

Step 5: Replace the GFCI if Necessary

If the outlet has noticeable damage, such as discoloration on the face, cracking or warping, if plugs are loose or fall out easily or if there has been exposure to water, replacement is necessary.

If your GFCI still won't reset after following these steps, it may be time to call a licensed electrician. Safety always comes first.


Why Reset Lockout Matters

GFCI in Kitchen

Reset Lockout isn't a nuisance; it's a lifesaving feature. By refusing to reset under unsafe conditions, your GFCI outlet helps prevent:

  • Electrical shock
  • Electrical fires

Understanding how this feature works empowers you to troubleshoot confidently and restore power safely.

Whether you're a homeowner trying to get an outlet working again, a DIYer learning the basics, or a contractor brushing up on electrical safety, knowing how reset lockout works is essential. It's one of the simplest yet most important safety features in a home electrical system.

Want to Learn More?  Watch our video series on the features and benefits of GFCI outlets

YouTube Video