Loading...
Wallplates

How to Choose the Right Wallplate for Your Home

Generally speaking, most people don’t pay much attention to their wallplates until it’s time to replace a device or paint a room. But the truth is wallplates are required for safety reasons by the National Electrical Code ® to protect people from any exposed area of an installed device and should be selected with care. They also add a finishing touch so switches, outlets, and lighting controls can seamlessly blend in with the room or accent decor. In some cases, wallplates are packaged with the device, but typically they are sold separately giving homeowners the opportunity to put some thought into appearance of their electrical devices.

Wallplates are available in a broad selection of configurations, as well as in the form of outdoor weather resistant covers, so whether you're updating a single switch or a larger multi-gang intsallation, wallplate material can often be changed without altering the existing device configuration. They are generally constructed of plastic, unbreakable thermoplastic or stainless steel and are available in Screwless standard, Standard, Midsize, and Oversized.

Wallplate Materials

Wallplates are available in different materials to withstand various usage patterns. The most common materials and their applications are outlined below:

Thermoset (Plastic)

Thermoset wallplates are suitable for most household applications. They are designed to resist fading, discoloration, grease, oil, organic solvents, moisture and scratches.

Thermoplastic (Nylon)

While both thermoset (plastic) and thermoplastic (nylon) wallplates offer long-lasting performance, nylon wallplates provide maximum resistance to impact. They are unbreakable and their added durability makes them ideal for high-traffic areas such as kitchens, bathrooms, family rooms and children’s bedrooms.

Metal

Metal wallplates stand up to heavy use, are easy to clean and their corners have rounded edges to help prevent injury and wall damage. Metal wallplates are available in a wide variety of metals including stainless steel, polished brass, brushed brass, chrome and aluminum. They're ideal for basements, garages, workshops, and utility rooms.

Antimicrobial Treated Wallplates

To combat the spread of germs, Leviton has developed antimicrobial treated wallplates that work to reduce the growth of bacteria. These wallplates are protected with a polyurethane powder coating that is embedded with a silver ion additive. The powder coating resists development of mold, mildew, fungi and other odor-causing bacteria as well as fingerprints and scuffing. Created with healthcare, childcare, food service, and hospitality applications in mind, they are also beneficial in home environments.

Wallplate Sizes

As with wallplate materials, wallplates come in various sizes to accommodate different needs. The size of the opening for the switch or outlet is always the same; the surrounding area is what varies.

Screwless, Standard features a snap-on cover for a clean, seamless look.

Standard is the most popular size for general use. 

Midway is slightly larger on all sides to help cover wall imperfections.

Oversized is notably larger on all sides to help cover more significant wall imperfections.

And if you have multi-gang installations simply add 1.81” (46.00mm) to the length of the wallplate for each additional gang.

Wallplate Sizes
Wallplate Configurations

You may be surprised to see the sheer number of wallplates in the electrical aisle and as you browse through them you suddenly realize that not all outlets are created equally. There are wallplates for single and multi-gang switches, combination outlets and switches, phone and cable outlets and even decorative outlets such as the Leviton Decora® line of devices, lighting controls and GFCI/AFCIs. Illustrated below are some common configurations found in today’s homes.

Wallplate Configuration
Extra Protection

Outdoor devices require extra protection and that’s where Weather-Resistant Outlet Covers and Extra Duty While-in-Use Covers come into play. Weather-Resistant Outlet Covers protect outdoor wiring devices from inclement elements. They are designed to close securely over the outlet and to be lifted up when the outlet is needed for use. Leviton Extra Duty While-in-Use Covers comply with the 2014 National Electrical Code® for “extra duty” application hoods for outlets in damp or wet locations. They also protect outdoor outlets from the elements but allow the outlets to remain covered while being used through built-in circular cord openings.

 

 

Combining Safety and Style

When selecting wallplates, it's important to consider both functionality and appearance. While wallplates are required to help cover exposed areas around electrical devices, they also contribute to a room's overall aesthetic. With a variety of materials, colors, and sizes available, homeowners can choose wallplates that complement their decor while providing the protection and durability needed for everyday use. From standard designs to decorative options, the right wallplate can help create a polished, finished look throughout the home.

To learn more, visit Leviton Wallplates