Loading...

New My Leviton Pro Support and Rewards Program Available for Smart Home Installers

Through the updated My Leviton app, pros can set up customers’ smart homes to earn and redeem awards points

Melville, NY, September 1, 2020 – Leviton announced today that the company is now accepting applications for My Leviton Pro – a new support and rewards program geared toward professional installing contractors. The program is available through the My Leviton app for Decora Smart Wi-Fi devices, which has been updated on iOS and Android platforms. The app now includes a special login for professional electricians and integrators, an exclusive 1-800 support number, and easy-to-earn rewards.

“The new My Leviton Pro Support and Rewards Program further ensures that our valued  electrical installation partners have the modern tools they need to effectively and efficiently turn every home into a smart home,” said Greg Rhoades director, marketing for Leviton. “For nearly 115 years, Leviton has assisted professional electricians, and our new My Leviton app features are just another way to show our appreciation and commitment to our partners.”

Through the new program, reward points are earned automatically upon Decora Smart Wi-Fi device enrollment to the My Leviton cloud – there are no invoices to submit and the points accrue almost immediately. With Pro Mode in the My Leviton app, electricians can use their own smartphones or tablets to log into their Pro accounts, create the homeowner’s residence, add smart devices to the cloud, and then transfer control of the devices in the home to the homeowner. Reward points vary based upon the complexity and cost of the My Leviton-compatible device, and points expire two years after a device is enrolled.

At any time, the owner or administrator can use the My Leviton app to redeem gift certificates to the Leviton Logo Store in increments of $25, $50, $75, or $100. Redeemed gift certificates expire a year after receipt, ensuring long-term accrual is possible to earn the higher-value gear from brands like Carhartt, Nike, Titleist, Otterbox, Under Armour, Swiss Army, and more. Additionally, a rewards tracking dashboard provides a historical reference of when points were earned and what smart devices were enrolled. Beyond on-demand rewards, grand prizes will also be randomly raffled, including – YETI coolers, and a trip to New Orleans to meet the development team for a private dinner and ride in a real Mardi Gras parade with hotel, air, and beads provided.

In addition to the pro program and features, all My Leviton app users can now enjoy several new user experience enhancements to the popular app:

  • A modernized and improved look, with the option to customize icons for smart devices and activities, such as “Movie Time”
  • Access and updated new firmware for all My Leviton devices in one place
  • Status of residence and lights, plus the option to easily engage home/away with the new “At a Glance” dashboard feature on the improved home screen
  • Ability to turn lights on and off with one tap, instead of two
  • Faster streamlined device setup with new illustrations and instructions.
     

These new features are coupled with all the great existing features, such as custom device settings, control from anywhere, schedules, activities, and integrations.

The My Leviton Pro Program is now accepting applications from US-based electrical contracting companies at http://my.leviton.com/pro and inquiries may be sent to MyLevitonPro@leviton.com. Upon approval, a Pro-level My Leviton app login will be provided, and the company owner or administrator may use the app to invite their electricians to earn reward points.

For more information about the My Leviton Pro rewards program, please visit: http://my.leviton.com/pro.  

About Leviton

Every day, Leviton is engineering possibilities that make the future happen, meeting the needs of today’s residential, commercial, and industrial customers globally. From electrical, to lighting, to data networks, and energy management, Leviton develops thoughtful solutions that help make its customers' lives easier, safer, more efficient and more productive. Driven by its commitment to its customers, the ingenuity of its employees and the safety and quality of its products and solutions, with Leviton, the FUTURE IS ON. For more information, visit www.leviton.com, www.facebook.com/leviton