Loading...

Leviton Announces ADVENTUM™ Fiber Cable for the EMEA Region

UK-made ADVENTUM cable builds on the success of the North American product line to expand Leviton's global fiber systems for premises applications

Bothell, WA, April 19, 2023 – Leviton Network Solutions' ADVENTUM Dry Water Blocked Indoor/Outdoor Multi Loose Tube cable is an innovative product that spans indoor and outdoor environments. The gel-free, advanced water-blocking technology, increased flexibility, and a ruggedized design withstands the rigors of outdoor environments while offering exceptional fire performance in all Euroclass environments. ADVENTUM is now made in Leviton's Glenrothes, Scotland factory. Leviton is building on years of success already achieved with this product in North America from Leviton’s Fuquay-Varina, NC factory.

ADVENTUM cable's comprehensive fire performance allows global customers to install in virtually any environment, including campus installations, internal building applications, vertical riser installations and data centers. ADVENTUM cable also provides optimal total cost of ownership for financial, health care, government, transportation, and education environments all over the world. The fiber optic cable can be installed from "closet-to-closet" among buildings, reducing the material and labor costs associated with building transition points by 25%.

"This latest addition to the ADVENTUM family is a versatile indoor/outdoor fiber cable with outstanding fire performance for European and international customers," said Richard Budd, senior product manager at Network Solutions Europe. "ADVENTUM is Leviton’s solution for the growing need for true universal, high fire-performance cabling, combining all the mechanical and environmental features of a traditional loose tube cable, with the added benefit of being gel free."

ADVENTUM CPR rated cables are made using 100% renewable energy in Leviton’s PAS2060 carbon neutral manufacturing facility in Glenrothes, UK, and are available in 12-144 fiber configurations in Single-mode, OM3, OM4 and OM5 versions. ADVENTUM cables are part of Leviton’s standard performance SDX Premises system, an OPT-X™ fiber system with spliced or mechanical field terminated connectivity to meet a wide variety of application needs and deployment locations for customers globally. To learn more, visit Leviton.com/ADVENTUM.

###

About Leviton Network Solutions
Leviton Network Solutions is a single-source global manufacturer of copper and fiber cabling systems. Leviton solutions are used in data centers, businesses, schools, hospitals, government facilities and commercial mixed-use markets around the world. All Leviton products are engineered to exacting standards, offer industry-leading performance and are backed by the industry’s best service and support. IT management, builders, contractors, and other industry professionals consistently rank Leviton products as the most preferred brand in the industry. We can expand your network possibilities. Learn more at www.leviton.com/ns or www.twitter.com/LevitonNS. European customers can visit leviton.com/ns/emea or twitter.com/LevitonNS_EU.