Loading...

Do Sensors Require Special Wiring?

Most sensors have been designed to use existing wiring and do not require a neutral for installation. See below for ground/neutral requirements for specific sensor models:

 

Product

Ground Required?

Neutral Required?

IPS02/IPV02

Yes

No

IPS05/IPV05

Yes

No

IPS06

Yes

No

IPSD6/IPVD6

Yes

No

IPS15/IPV15

No

Yes

IPHS5

No

Yes

DOS02/DVS02

Either Neutral or Ground Required

Either Neutral or Ground Required

DOS05/DVS05

Either Neutral or Ground Required

Either Neutral or Ground Required

ODS10

Yes

No