Loading...

What is an arc-fault?

An arc-fault is an unintentional arcing condition in a circuit. Arcing creates high-intensity heating at the point of the arc, resulting in burning particles that can exceed 10,000 degrees Fahrenheit and may over time ignite surrounding material such as wood framing or insulation.

There are two types of potentially dangerous arcs – parallel arcs and series arcs.

Arc-Fault