NOTE: Activation of RFID access control is ONLY required when access to charging will be restricted only for RFID card holders. If no restriction is required (open charging) this step is NOT required.
1. Identify Your Card
- All units come with 1 administrative (admin) card and 2 standard cards as marked on the cards
- Admin cards are used to activate RFID access control and should be kept by charger owner
- Standard cards are used to enable charging by users
2. Activate RFID Access Control
WARNING: Once enabled, RFID access control cannot be disabled. If you prefer to keep this as an unrestricted unit, do not activate this card.
- To enable RFID access control, hold the admin card to the RFID sensor image on the front of the charger until you hear a beep. RFID access control is now enabled.