Loading...

Can I Toggle More Than One Light From A Scene Controller Button?

Scene Controller buttons can be configured for ON / OFF toggle control of an individual Decora Smart Wi-Fi device.  On/Off toggle control using one button for a group of lights is not supported.

A scene controller button can be configured to run a Scene and this is the best solution for controlling multiple devices.

Locate the card for the D2SCS or DW4BC and then tap the three dots in the upper right corner.  Tap the button you would like to program and tap Yes to confirm that this is the button you would like to program.    

Devices
Devices
Devices

Select Set Keypad Scene 

Devices

Select the devices that you want to program to this button and then tap Next

Devices

Now set the state of the devices, ON / OFF / Dim Level, etc. and then tap Next

Devices

Enter a name for the button and then tap Save.

Devices
Devices