Loading...

LaGuardia Case Study

Leviton installed 75 custom-made GreenMAX Panels throughout the terminal. 

LaGuardia Aiport departures hall

Modernizing Airport Lighting Controls to Meet Travel Demands and Energy Codes

The Challenge

A vital part of the NY transportation system, LaGuardia Terminal B needed to be modernized to meet the needs of travelers. Desperately in need of upgrades, airport officials took on a massive 6-year renovation project, including a new terminal to meet passenger demands and energy codes. Officials also had to ensure operations were not interrupted.

The Installation
Custom GreenMAX Lighting Control Relay Panels, networking equipment, Sapphire™ Touch Screens, emergency controls, and Leviton standalone products were installed as part of the upgrades. The entire system was ultimately tied into the terminal’s BMS system resulting in no downtime or interruption of services despite multiple phases of the project.

The Solution
Leviton installed 75 custom-made GreenMAX Panels throughout the terminal. Each panel was equipped with a main circuit breaker and 0-10V dimming relays determined by the consulting engineer. Commercial tenants in Terminal B had Sapphire Touch Screens installed to provide scene, scheduling, and preset controls.

Leviton Multi-Tech Ceiling Mount Occupancy Sensors were installed to keep the lights on when needed and in accordance with energy codes.

Leviton daylight harvesting and energy saving photocells were added to Terminal B which is brightly lit with floor-to-ceiling windows. The result is a seamless integration of a modern code-compliant lighting control system that enhances the passenger experience and state-of-the-art architecture.

The result is a seamless integration of a modern code-compliant lighting control system that enhances the passenger experience and state-of-the-art architecture.

GreenMAX Relay Panels
GreenMAX offers unlimited and flexible lighting configurations that are easy to monitor, manage, and maintain while meeting energy code requirements regardless of the project size.This centralize lighting control powerhouse features dimming,partial-ON, partial-OFF, advanced scheduling, demand response, and daylight harvesting capabilities.

Sapphire Touch Screens
Combine the easy system integration of Leviton commercial lighting controls with the flexibility of a customizable user interface and native control convenience.Sapphire provides an elegant, full-scale touchscreen control solution for dimming, scene control, scheduling, occupancy sensing, daylighting, and color tuning.

Multi-Tech Occupancy Sensors
Self-adjusting internal microprocessor continually analyzes, evaluates, and adjusts the sensitivity and time delay.

Photocells
Leviton photocells precisely monitor either task or ambient light levels. Photocells work with other components in the system to automatically adjust light levels to a user defined level.

Leviton offers spec-ready and code-compliant lighting and control solutions for airport terminal applications for seamless installations and energy savings.

Leviton Solutions