Loading...

What is a Mechanical Interlock?

What Are Mechanical Interlocks?

In industrial and commercial electrical systems, safety is key when connecting and disconnecting power.  A mechanical interlock is a built-in safety mechanism that physically controls the sequence of operation to help prevent unsafe conditions.

Leviton mechanical interlocks are designed to ensure that power circuits are disconnected before a plug can be removed and prevent plugs from being inserted while the circuit is energized.  This helps protect personnel, equipment, and operations from potential electrical hazards while supporting safe, reliable power distribution.

How Do Mechanical Interlocks Work?

A mechanical interlock uses a physical locking mechanism integrated into a receptacle, disconnect switch, or power distribution device.  The interlock enforces a specific sequence of operation by preventing certain actions until predefined conditions are met.

For example, in a Leviton switched interlocked receptacle:

  1. The receptacle must be switched OFF before the plug can be inserted or removed.
  2. Once the plug is fully engaged, the switch can be turned ON to energize the circuit.
  3. To disconnect power, the switch must first be returned to the OFF position.
  4. The plug can then be safely removed.

This sequence helps eliminate the possibility of connecting or disconnecting equipment under load, reducing the risk of arcing, equipment damage, and personnel injury.

Where Are Mechanical Interlocks Used?

Mechanical interlocks are commonly used in applications where safe equipment connection and disconnection are critical, including:

  • Manufacturing facilities
  • Food and beverage processing plants
  • Water and wastewater treatment facilities
  • Mining operations
  • Oil and gas facilities
  • Transportation and infrastructure projects
  • Temporary power and portable equipment applications

These environments often require frequent equipment connection and disconnection, making proper load interruption essential for safe operation.

Explore Leviton mechanical interlocks for commercial and industrial applications at leviton.com/levseries