Loading...

The Future of Wiring is Here with Leviton's Lever Edge™

Leviton Lever Edge Product

Nowadays, time is money. Getting the job done as quickly and safely as possible is key for a contractor. Any tool or product that helps get things done even faster is one you'll want to add to the back of your work truck.

Leviton's comprehensive line of Lever Edge procudts provides an innovate new UL approved termination method to make installing outlets and switches faster, easier, and safer. Lever Edge products feature an industry-first screwless, self-grounding reusable wire termination that accepts 12 and 14 gauge, solid and stranded wires. This revolutionary product is designed with contractors in mind to help get jobs done quicker so you can spend more time on other projects and business.

Why Lever Edge?

Lever Edge dramatically decreases installation time by simplifying the process to three quick steps:

  1. Push - Ensure the lever is open and press the stripped end of a wire into the correct color-coded terminal
  2. Click - Close the lever and confirm the right connections are made with an audible click.
  3. Done - Complete the connection with confidence!

The Benefits

Compared to conventional wiring devices where a terminal screw is present, Lever Edge has a unique color-coded lever termination feature. The hot, neutral and ground wire terminals are color-coded, making it easier then ever to identify the correct terminal for wiring. This innovative connection method also makes handling boxes with short existing wires more convenient. 

Lever Edge is the only electrical wiring device on the market with a quick termination ground wire and a strap that is compatible with any sized wallplate. Safety is also built-in to Lever Edge. There are no exposed metal parts, eliminating the need to use electrical tape and lessening the likelihood of electrical mishaps. 

Contractors and electricians are beginning to take advantage of Lever Edge to speed up installation positively impacting their day-to-day work. Other key benefits include:

  • Seamless coordination with Leviton's Decora® family of products
  • Can be used with midway and standard wallplates and Decora Plus™ screwless wallplates.
  • A larger strap with a unique tongue and groove alignment feature that offers quicker trim out and alignment on multi-gang installations.
  • Lever Edge is UL Listed, so contractors can ensure they are meeting the appropriate electrical standards.

The Bottom Line

Lever Edge is revolutionizing the way contractors and electricians install outlets and switches. Time spent on projects will dramatically decrease, bringing further improvements in overall efficiency on the jobsite. Learn more about Lever Edge and check out Leviton's YouTube channel.