When temporary power is needed, extension cords are often the first solution that comes to mind. However, for construction sites, industrial facilities, and other demanding environments, portable outlet boxes can offer a more organized and efficient way to distribute power. Leviton's Portable Outlet Boxes are designed specifically for temporary power applications and can help bring power exactly where it's needed.
Portable Outlet Boxes vs. Extension Cords: Which Is the Better Temporary Power Solution?
Portable Outlet Boxes vs. Extension Cords
Extension cords extend power to equipment, while portable outlet boxes can be incorporated into temporary power assemblies to provide one or more receptacle points closer to the work area.
Portable Outlet Boxes
- Multiple outlets from a single power source
- Power several tools or devices at once
- Help reduce cord clutter and improve organization
- Designed for temporary power applications with standard and weather-resistant cover options
Extension Cords
- Often used to extend power to one device or work area at a time
- May require additional cords or adapters for multiple devices
- Convenient for simple, short-term application
- Can become harder to manage in larger work areas
Conclusion
Both portable outlet boxes and extension cords have their place, but the right solution depends on the application. While extension cords are convenient for basic temporary power needs, portable outlet boxes provide a more robust solution for environments that require multiple outlets, improved organization, and reliable temporary power distribution. For construction sites, manufacturing facilities, and other demanding applications, a portable outlet box can help bring power exactly where it's needed.
Note: Temporary power components should be properly rated for the load and environment, assembled and installed according to applicable instructions and requirements, and inspected before use.