Whether you're developing a new RV park, upgrading an existing campground, or evaluating options for a single RV site, selecting the right RV power pedestal is essential. The right pedestal does more than provide electricity. It can also support lighting, water access, metering, and overall site convenience while standing up to years of outdoor exposure. Leviton's RV power pedestals are designed to bring power throughout RV parks and campgrounds while offering customizable features to meet a wide range of site requirements.
How Do I Choose the Right Power Pedestal for My RV Site?
Start with Your Power Requirements
One of the first factors to consider is the amount of power your RV sites need. Different RVs have different electrical demands, so it's important to select a pedestal configuration that matches the types of vehicles using your campground. Understanding the various types of electrical pedestals available helps ensure guests have reliable access to power while minimizing future upgrades.
In some applications, campground owners may also evaluate metering solutions depending on site design and utility requirements.
Explore available options on Leviton's RV Power Pedestals page.
Look Beyond Power: Water, Lighting, and Metering
Today's RV parks often need more than electrical service. Many RV pedestal configurations can include:
- Water hook-up options
- Analog water and kW metering
- Daylight-sensing LED lighting
- Standard breaker protection
These integrated features can improve convenience for guests while helping operators monitor utility usage and improve site management. Leviton's RV power pedestal solutions offer customizable configurations that allow campground owners to choose the combination of services that best fits their operation.
Consider Weather and Location
RV sites are exposed to the elements year-round, making durability a critical consideration. When evaluating an outdoor electrical pedestal installation, look for features designed for demanding outdoor environments. Depending on the application, important characteristics may include weather-resistant enclosures, corrosion-resistant materials, lockable covers, and NEMA-rated protection.
Leviton's RV power pedestal solutions are designed with durability in mind and include features such as NEMA 3R-rated construction, lockable self-closing covers, and rugged materials built to withstand outdoor conditions.
Customization Matters
No two RV parks are exactly alike. Site layout, occupancy levels, utility requirements, and regional regulations can all influence pedestal selection. That's why many campground owners choose customizable pedestal solutions that can be configured with different receptacles, power ratings, metering options, lighting, and other site-specific features.
In some mixed-use environments, property owners may compare an RV vs marine pedestal solution. While both provide reliable outdoor power distribution, RV pedestals are specifically designed around campground and recreational vehicle applications, while marine pedestals are engineered for dockside shore power and waterfront environments.
Don't Overlook Maintenance
Long-term reliability often depends on ease of service. Features that simplify wiring access and inspections can help streamline electrical pedestal maintenance and reduce downtime over the life of the installation. Leviton's RV pedestal solutions are designed with easy wiring and maintenance access to support ongoing operation.
Choosing the Right Solution
From basic campsite power to fully featured utility stations with lighting, water, and metering capabilities, the right RV power pedestal can enhance the guest experience while supporting efficient campground operations. Whether you're comparing a meter pedestal, evaluating types of electrical pedestals, or planning an outdoor electrical pedestal installation, choosing a durable, customizable solution can help protect your investment for years to come.
To learn more about Leviton's complete line of RV and campground power solutions, visit the RV Power Pedestals page or browse the full Power Pedestals portfolio.