Loading...

New Leviton GreenPack® Packaging Streamlines Installation and Reduces Material Waste

New recyclable bulk connector packaging saves on installation time while decreasing material waste at jobsites

Bothell, WA, April 3, 2019 – IT network managers constantly seek more efficient and cost-effective options for large connector installations. Leviton today announced new GreenPack® packaging that supports these efforts while contributing to an organization’s environmental initiatives.

The bulk packs — available for select Atlas-X1® and eXtreme® RJ-45 connectors — hold 12 connectors in individual, clear pockets. The connectors can be removed quickly, one at a time, with remaining connectors and components well organized and easily counted. The packs offer an environmentally sound alternative to individually packaged jacks, and the corrugated cardboard sleeve and PET plastic packaging is 100 percent recyclable

“The innovative GreenPack packaging is easy to open, reusable and generates more jobsite efficiency with less waste,” said Yuna Shin, senior product manager for Leviton Network Solutions. “These benefits are especially noticeable in larger installations: In a typical 10,000 connector installation, using GreenPack provides a 3 percent total project cost savings in materials and labor.”

The bulk packaging is available for Atlas-X1 Cat 6A and Cat 6 UTP and shielded connectors, and eXtreme Cat 6A UTP connectors.

  • GreenPack saves time on the jobsite, enabling faster unpacking and deployment versus individually bagged connectors.
  • The packaging features secure corner tabs that open and close easily and create added protection for all connector components.
  • A see-through window on GreenPack boxes allow for quick product identification.
  • GreenPack is available in three connector colors for better network planning.
  • Atlas-X1 and eXtreme connectors are compatible with all Leviton QuickPort® products.
  • A 12-connector GreenPack provides the right number of connectors to match patch panel configurations (12 ports = 1 Pack, 24 ports = 2 Packs, 48 ports = 4 Packs).

Leviton is dedicated to conserving resources to preserve the environment for future generations. In fact, its Network Solutions facilities are ISO 14001:2015 certified to ensure its environmental impact is being measured and improved.

Leviton connectors, including those sold in the new GreenPack, are available through the company’s extensive distribution network.

For more information, visit www.leviton.com/coppersystems.

About Leviton Network Solutions
Leviton Network Solutions delivers complete network structured cabling systems for data center, enterprise, education, health care, government and commercial mixed-use markets around the globe. Solutions include copper and fiber optic connectivity, IT/AV systems, and much more. All Leviton products are engineered to exacting standards, offer industry-leading performance and are backed by the industry’s best service and support. IT management, builders, contractors and other industry professionals consistently rank Leviton products as the most preferred brand in the industry. We can expand your network possibilities. Learn more at www.leviton.com/ns or www.twitter.com/LevitonNS. European customers can visit www.brand-rex.com or www.twitter.com/LevitonNS_EU.

About Leviton
Every day, Leviton is engineering possibilities that make the future happen, meeting the needs of today’s residential, commercial, and industrial customers globally. From electrical, to lighting, to data networks, and energy management, Leviton develops thoughtful solutions that help make its customers' lives easier, safer, more efficient and more productive. Driven by its commitment to its customers, the ingenuity of its employees and the safety and quality of its products and solutions, with Leviton, the FUTURE IS ON. For more information, visit http://www.leviton.com/, www.facebook.com/leviton, www.twitter.com/leviton, or www.youtube.com/Levitonmfg.