Loading...

Print Leviton Introduces Type A and Type-C™ USB Charger/Tamper Resistant Receptacle

Latest addition to USB Charger Devices product line is designed for maximum charging efficiency

Melville, N.Y. January 02, 2018 -

Leviton today announced the most powerful addition to its line of USB Charger Devices. The Type A and Type-C™ USB Charger/Tamper Resistant Receptacle offers two high powered vertical USB ports, one Type A and one Type-C, delivering a combined total of 5.1A charging current and 25+ watts of power, along with two additional tamper resistant receptacles.

The Type-C port within the receptacle provides up to 59 percent faster charging power compared to leading competitors based upon tests performed using a Lightning® cable and the Type-C port with an iPhone® 7, iPad Mini™ 1 and iPad Pro® 9.7. Engineered utilizing smart chip technology, the device recognizes and optimizes the charging requirements of individual devices for faster charging of smartphones, tablets and other peripheral devices that use the Type-C cable.

“The Leviton Type A and Type-C™ USB Charger/Tamper Resistant Receptacle delivers faster, more powerful charging to a wide range of electronic devices, and the reversible Type-C connector allows users to easily plug in cables in either direction,” said William Randall, director of product management, Leviton Residential. “The addition of two tamper resistant receptacles not only improves child safety, but also provides a convenient solution for other power needs while devices are charging.”

With a 5-year limited warranty, Leviton Type A and Type-C™ USB Charger/Tamper Resistant Receptacles are ideal for residential and commercial applications including kitchens, bedrooms, college dormitories, airport lounges, hospitals (hospital grade model available), salons and spas, hotels, meeting rooms, cafes, restaurants and more. Combining functionality with style, the device is available in white, ivory, light almond, gray, black, brown and red, and is compatible with the complete line of Leviton Decora® wiring devices, Decora wallplates and Decora Plus™ screwless wallplates.

The Leviton Type A and Type-C™ USB Charger/Tamper Resistant Receptacle is now available through Leviton’s network of retail, online and electrical distribution channels, including its online store. For additional product information, visit www.leviton.com/usb.

About Leviton Residential

Leviton residential products are the brand most preferred by builders and electrical contractors. Leviton’s award winning lighting controls and wiring devices help electrical industry professionals and homeowners create smart and safe living environments that deliver energy savings, convenience and reliability. Learn more at www.leviton.com/residential.

About Leviton

Leviton is the smart choice, delivering the most comprehensive range of solutions to meet the needs of today’s residential, commercial and industrial customers in more than 90 countries across the globe. From simple switches and receptacles, to networking systems and smart home automation, Leviton exceeds market needs by delivering innovative products to create sustainable, intelligent environments through its electrical wiring devices, network and data center connectivity solutions, LED lighting and lighting energy management systems, and security and automation applications. For Leviton, it is clear the FUTURE IS ON. For more information, visit www.leviton.com, www.facebook.com/leviton, www.twitter.com/leviton, or www.youtube.com/Levitonmfg.