Loading...

Leviton Launches Enclosed Main Breaker Disconnect

Designed to meet NEC 2020 Section 230.85 requirements mandating exterior disconnect for residential applications

MELVILLE, N.Y., June 30th, 2025 – Leviton today announced the launch of its Enclosed Main Breaker Disconnect – the latest addition to the Leviton Load Center product line. The new solution is designed to help builders and contractors meet the latest National Electrical Code® (NEC) 2020 Section 230.85 requirement, which mandates an exterior disconnect for residential applications.

The Enclosed Main Breaker Disconnect provides a safe, code-compliant way to shut off power to an entire residence from outside the home – an essential feature for first responders during emergencies such as fires, floods or natural disasters. While the product is required for new construction in states that have adopted NEC 2020, it is ideal for all new residential construction[VL1] , renovation projects requiring electrical upgrades, and for those seeking to future-proof installations with the latest safety features.

“Leviton is committed to delivering innovative solutions that form the backbone of safe and efficient electrical systems,” said Aaron Ard, vice president of product management for Leviton. “Our new enclosed main breaker disconnect is designed to meet the growing demand for reliable, code-compliant solutions. Whether supporting new construction, system upgrades or code requirements, this product empowers homeowners and professionals alike with greater control and confidence in their electrical infrastructure.”

Designed to offer customization and flexibility, Leviton’s Enclosed Main Breaker Disconnect is available with or without a 200A main breaker included, allowing contractors to install a main breaker with an amperage rating of their choosing. Both product versions include NEC-approved labeling for Service and Emergency Disconnect applications. The Enclosed Main Breaker also works seamlessly with other manufacturers’ main service panels, in addition to Leviton Load Centers.

Leviton Load Center Advantage

The new Enclosed Main Breaker Disconnect products expand on Leviton’s existing portfolio of durable and easy-to-install load center solutions. Leviton circuit breakers feature a plug-on design, increasing productivity and reducing installation time by up to 25%. Also available with outdoor enclosures, Leviton panels can be installed in a variety of climates and are protected against environmental factors.

For more information about the Leviton Load Center, and to explore Leviton’s full range of electrical products, visit Leviton.com/loadcenter.

About Leviton

Every day, Leviton builds what’s next to light, power, and connect everyday spaces to meet the needs of its residential, commercial, and industrial customers globally. From controls, to lighting, to electrical, to networking, Leviton’s relentless innovation for more than a century enables our customers' lives to be easier, safer, more efficient, productive and sustainable. Driven by its commitment to its customers, the ingenuity of its employees, and the safety and quality of its products and solutions, with Leviton, the FUTURE IS ON. For more information, visit http://www.leviton.com/, www.facebook.com/leviton, www.x.com/leviton, or www.youtube.com/leviton.