News Summary
· Modern electronics can produce complex electrical signatures that can resemble fault conditions, resulting in unnecessarily tripped breakers, or “nuisance tripping.”
· Leviton's new TrueArc AFCI technology combines advanced sensing capabilities and machine learning-based analysis to help distinguish routine electrical activity from potentially hazardous arc-fault conditions.
· TrueArc technology is available in Leviton AFCI and Dual Function AFCI/GFCI breakers for Leviton Load Centers.
MELVILLE, N.Y., October 14, 2026 – Leviton today announced the launch of TrueArc™ AFCI Technology, a next-generation advancement in AFCI circuit protection now available in Leviton AFCI and Dual Function AFCI/GFCI breakers for Leviton Load Centers. Developed through years of research, development, testing and real-world field evaluation, this technology helps prevent unnecessary tripping resulting from electrical signatures that resemble faults, or nuisance tripping, while maintaining protection that meets UL 1699 AFCI requirements and supports NEC® AFCI compliance requirements.
Leviton’s new TrueArc AFCI Technology is engineered to minimize nuisance tripping and has been extensively tested in real-world field installations across the United States and Canada.
As homes utilize more electronics, connected devices, LED lighting, efficient appliances, EV chargers and switching power supplies, their increasingly complex electrical signatures can resemble fault conditions. TrueArc technology provides advanced circuit protection that can better distinguish normal electrical activity from a genuine arc fault with maximum efficiency. This helps prevent contractors from having to take troubleshooting phone calls from homeowners or making site callbacks.
"Electrical professionals have made it clear that reducing nuisance tripping remains one of the biggest opportunities for improvement in AFCI protection," said Aaron Ard, Vice President of Residential Product Management at Leviton. "TrueArc technology delivers the performance contractors have been asking for, significantly reducing nuisance tripping, while maintaining the protection required by modern safety standards. It's a no-nonsense AFCI solution built for today's homes and tomorrow’s electrical loads."
TrueArc AFCI technology combines a newly developed high-resolution sensing platform with a powerful processor that uses machine learning-based classification to continuously evaluate electrical patterns. By providing more information for analysis, the enhanced platform helps the breaker distinguish normal appliance operation and complex electronic loads from conditions that may indicate a true arc-fault hazard.
To validate performance, Leviton conducted extensive field trials with electrical professionals throughout North America and collaborated with major appliance manufacturers to evaluate compatibility across a broad range of residential electrical loads. The technology was specifically developed to improve immunity to common contributors to nuisance tripping, including high-frequency electrical noise and activity occurring on neighboring circuits.
The result is a future-ready AFCI platform designed for modern homes filled with electronics and sophisticated electrical loads. By better distinguishing normal appliance behavior from genuine fault conditions, TrueArc technology can help electrical professionals reduce troubleshooting visits and callbacks, improve homeowner satisfaction and spend less time diagnosing unwanted trips.
For more information, visit Leviton.com/NoNonsense.
Frequently Asked Questions
Q: Which products feature TrueArc technology?
A: TrueArc technology is available in Leviton AFCI and Dual Function AFCI/GFCI breakers for Leviton Load Centers, including standard and Smart 15A and 20A one-pole configurations.
Q: Does TrueArc still meet AFCI safety requirements?
A: Yes. TrueArc AFCI breakers continue to comply with UL 1699 AFCI requirements and support NEC AFCI compliance requirements.
Q: Why was TrueArc developed?
A: Modern homes contain more electronics, smart home devices, LED lighting, appliances and electrically complex loads than ever before. TrueArc was developed to improve compatibility with these evolving residential electrical environments while maintaining arc-fault protection.
About Leviton Residential
Leviton residential products are the brand most preferred by builders and electrical contractors. Leviton’s award-winning load centers, lighting controls and wiring devices help electrical industry professionals and homeowners create smart and safe living environments that deliver energy savings, convenience and reliability. Learn more at www.leviton.com.
About Leviton
Every day, Leviton builds what’s next to light, power, and connect everyday spaces to meet the needs of its residential, commercial, and industrial customers globally. From controls, to lighting, to electrical, to networking, Leviton’s relentless innovation for more than a century enables our customers' lives to be easier, safer, more efficient, productive and sustainable. Driven by its commitment to its customers, the ingenuity of its employees, and the safety and quality of its products and solutions, with Leviton, the FUTURE IS ON. For more information, visit http://www.leviton.com/, www.facebook.com/leviton, www.x.com/leviton, or www.youtube.com/leviton.