To reset Decora Smart Zigbee device to factory settings and place into joining mode:
- Hold the top of the paddle (if wall switch) or back-lit button (if plug-in device) for a total of 14 seconds.
- After the first 7 seconds the light turns amber. Continue to hold.
- After a total of 14 seconds, the status light will quickly flash red/amber.
- Release the top of the paddle (if wall switch) or back-lit button (if plug-in device) and the Decora Smart Zigbee device will reset.