Loading...

Including a Decora Smart® Z-Wave Device onto a Z-Wave Network

Leviton Decora Smart Z-Wave devices support two methods of inclusion. When using a Z-Wave Plus certified controller choose Network Wide Inclusion. If network wide Inclusion does not discover your device, please try traditional inclusion.


Network Wide Inclusion:
Network Wide Inclusion allows your device to be included into the network using devices already in the network to assist with communication. Work your way from the closest devices to the controller outward.

  • Enter Programming Mode by holding the top of the paddle for 7 seconds (the Locator LED will turn amber), and then release (the Locator LED will begin to blink amber).
  • Tap the top of the paddle one time. The Locator LED will quickly flash green.
  • The Decora Smart Z-Wave device is ready to be included into the Z-Wave network.
  • Follow directions in the Z-Wave controller to complete the inclusion process.
    • Upon successful inclusion onto the Z-Wave network, the LED will turn off and then blink green 3 times.
    • If the inclusion process is not successful, the LED will flash red 3 times.

 

Traditional Inclusion:
For older controllers, Traditional Inclusion is supported. Depending on the age of the controller, the controller will need to be 3 to 35 feet from the device when including.

  • Enter Programming Mode by holding the top of the paddle for 7 seconds (the Locator LED will turn amber), and then release (the Locator LED will begin to blink amber).
  • The Decora Smart Z-Wave device is ready to be included into the Z-Wave network.
  • Follow directions in the Z-Wave controller to enter learn mode.
  • Tap the top of the paddle one time. The Locator LED will quickly flash green. The Z-Wave controller will begin to pair with the Decora Smart device.
    • Upon successful inclusion onto the Z-Wave network, the LED will turn off and then blink green 3 times.
    • If the inclusion process is not successful, the LED will flash red 3 times.