The Customer
The U.S. Securities and Exchange Commission oversees the key participants in the securities world, including securities exchanges, securities brokers and dealers, investment advisors, and mutual funds.
The Challenge
The SEC leased four floors of space in an established building and required a lighting control system capable of occupancy sensing, daylight harvesting, and time-based control. Additionally, scene capabilities in the conferecne room were required.
The Solution
To best meed their project requirements, the SectorFlex solution was chosen. SectorFlex allowed occupancy sensing, daylight harvesting, time-based control, and integration of scene control. The initial design used LED fixtures, which the Sector Relay is capable of driving with the 0-10VDC driver. During the value engineering process, the LED option was changed to fluorescent. The flexibility of SectorFlex allowed for this change with no system redesign required. To provide the SEC with their desired scene control, a Dimensions® D4200 Controller was specified. The protocol for the D4200 is Luma-Net; the Sector system uses the LumaCAN protocol. A LumaCAN Gateway was installed to convert the protocols, providing seamless system integration.
The Results
The flexibility of SectorFlex allowed the specified system to be connected to existing components from other manufacturers seamlessly to achieve the desired system requirements without additional equipment costs. The ease of installation due to the flexibility of the 2-wire signal buss provided a time and cost savings with the electrical contractor.
For More Information
To learn more about the wide range of Leviton’s lighting control and energy management solutions, please visit www.leviton.com/lms or call 503-404-5555.and energy savings.
| Location: | U.S. Securities and Exchange Commission Washington, DC, USA |
| Application: | SectorFlex relays Dimensions D4200 Gateway |
| Industry: | Government |
| System Components: | Occupancy Sensing Daylight Harvesting Scene Control Time-Based Control |
| Benefits: | Customers are happy with the new technology and fully utilize the dimming and daylight harvesting features. |
| General Contractor: | JE Richards |
| Architect: | GDA |
| Engineers: | TMR Engineering |
| Start to Finish: | April 2010 to December 2010 |